Short  Circuit Current Rating for Industrial Control Panels

Guidelines on the Short Circuit Current Rating

Since the 2005 edition, the NFPA70: National Electrical Code® (NEC) requires that industrial control panels have to
be marked with an appropriate short circuit current rating (SCCR). This became effective and mandatory in April 2006. The SCCR value in kA, at a defined voltage, is an indication of what fault current the industrial control panel can withstand(without unacceptable damage) in the event of a fault. Thus, the maximum fault current and the panel’s short circuit current rating should not be confused. Furthermore, an industrial control panel shall not be installed where the available fault current exceeds its short circuit current rating.

Fill out the information below to read the entire white paper. We'll notify when there are updates to the guidelines on SCCR for industrial control panels.