Loher Motors

Loher low-voltage motors have been specifically tailored to address extreme applications such as winch drives on the decks of ships, transporting and pumping natural resources from the depths of the sea, drilling units for tunnels and the mining sector, high and low temperature applications as well as especially production plants and machines located in hazardous areas in the chemical, petrochemical and oil & gas industries.Loher motors are available in all of the usual types of protection - also in double protection where there is an especially high danger of explosion.

Did this information help you?